PCA9420 Power Up and Operation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA9420 Power Up and Operation

4,264件の閲覧回数
Kevin23
Contributor II

I am using the PCA9420 PMIC with the RT685.  I need to be able to power up with only VBAT connected (no external voltage on VIN).  It appears a voltage on VIN is required for power up.  I am not using VIN directly because our input voltage was falling too close or hitting to the 3.1V UVLO on VIN and not powering up.  Is it acceptable to use the VBAT voltage with a diode connected to VIN for power up?

I will be inputting 3.3V on VBAT.  This will result with VIN being 3.0-3.1V with the diode drop.  In testing this appears to work as all regulator enable to the proper voltage and the SYSRST is released.  I know the VIN is close to the UVLO but does not seem to disable the regulator outputs if it falls below the default 3.1V VIN_UVLO.  The ASYS voltage should be valid and use the VBAT input as it is higher than VIN.  I plan on leaving the PMIC powered in the configuration (VIN powered by VBAT with diode).

Is this a valid power up and operational design?

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,976件の閲覧回数
GeoZh
Contributor II

Hi,Kevin!

I‘ve tested powering only the VBAT pin without powering the VIN. A battery(400mAh, 3.7-4.2V) was connected to VBAT.The PCA9420 worked properly in my case.This may be helpful to you.

0 件の賞賛
返信

4,259件の閲覧回数
Kevin23
Contributor II

Our VBAT input will be 3.0-3.6V.  

We had some confusion on the power up in section 8.10.3 of the datasheet. In condition 1, we though a valid voltage on VIN was required for power up.  We think inputting a voltage on VBAT, with VIN floating, will satisfy "A voltage on ASYS higher than ASYS_UVLO, a 2.8V typical" and should start the power up sequence.  Is this correct?

 

0 件の賞賛
返信

4,241件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

• A valid VIN supply on VIN pin
• A voltage on ASYS higher than ASYS_UVLO, a 2.8V typical

Please meet above these two conditions.

0 件の賞賛
返信

4,237件の閲覧回数
Kevin23
Contributor II

Both conditions must be met?  VIN must be supplied?  This seems odd for battery powered devices.  

In testing we are able to power up with just VBAT and no voltage on VIN.  ASYS will be powered by VBAT.

What is the valid voltage on VIN need for if a battery (VBAT) is attached?

0 件の賞賛
返信

4,260件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

which kind type of battery do you use in your case?

what's the voltage range of your battery?

 

0 件の賞賛
返信