NVT4858 - SDIO voltage translation for STM32F413

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NVT4858 - SDIO voltage translation for STM32F413

1,198件の閲覧回数
Thai1
Contributor I

Hi, 

On our PCB we are designing a microcontroller STM32F413 at 1.8V and are looking for a suitable level translator to 3.3V for the on-board microSD connector (diagram below). The microcontroller only supports up to SDIO v2.0 so we are not expecting to run SDIO in any UHS mode on this board. Would NVT4858 be suitable for our application?   

I also noticed NVT4858 has an optional clock feedback output. I guess it is not required for SD cards in non-UHS modes?

Thai1_0-1699376805977.png

Thai1_1-1699377142689.png

0 件の賞賛
返信
1 返信

1,169件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Thai1,

I hope all is great with you.

Is your question related to the following post?

https://community.nxp.com/t5/Other-NXP-Products/NVT4858-SDIO-voltage-translation-for-STM32F413/m-p/1...

Regards,

David 

0 件の賞賛
返信