MRF101AN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MRF101AN

1,383 Views
churujia
Contributor I

Can MRF101AN support 12v power supply? If so, how much power can be output?

0 Kudos
Reply
1 Reply

1,290 Views
LPP
NXP Employee
NXP Employee

MRF101AN could be used at low drain voltage, but, performance will be worse. My estimation is P1dB reduction by 7.7 times and gain -8dB (at 27MHz): 16Watt, 17dB.

NXP offers devices designed for 12V operation. I recommend AFT05MP075N or AFT05MS031N. AFT05MP075N provides 75W, 35dB, 70% efficiency in NXP 88-108MHz design at 12.5V.

https://www.nxp.com/products/rf/rf-power/rf-mobile-radio/136-520-mhz-70-w-12.5-v-broadband-rf-power-...

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply