MRF101AN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MRF101AN

1,361件の閲覧回数
churujia
Contributor I

Can MRF101AN support 12v power supply? If so, how much power can be output?

0 件の賞賛
返信
1 返信

1,268件の閲覧回数
LPP
NXP Employee
NXP Employee

MRF101AN could be used at low drain voltage, but, performance will be worse. My estimation is P1dB reduction by 7.7 times and gain -8dB (at 27MHz): 16Watt, 17dB.

NXP offers devices designed for 12V operation. I recommend AFT05MP075N or AFT05MS031N. AFT05MP075N provides 75W, 35dB, 70% efficiency in NXP 88-108MHz design at 12.5V.

https://www.nxp.com/products/rf/rf-power/rf-mobile-radio/136-520-mhz-70-w-12.5-v-broadband-rf-power-...

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信