MC33772B wake up by CSB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC33772B wake up by CSB

1,143件の閲覧回数
shiqi_seventeen
Contributor III

Hello, team.

I am currently using MC33772B and have encountered a problem. I can put the MC33772B into sleep mode, but I am having trouble waking it up using the CSB pin. I followed the manual and changed the CSB pin from low to high, but the MC33772B remains in sleep mode and is not waking up.

shiqi_seventeen_0-1720055967096.png

 

I was wondering if there's something I've missed or if I'm operating it incorrectly. Could you please help me with this?

0 件の賞賛
返信
1 返信

1,110件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

The tWAKE-UP time starts after a valid CSB wake-up pulse, so indeed it does not include the 65µs CSB wake-up de-glitch filter timing.

 

As for the minimum low pulse width, there is no requirement here.

In order for a CSB wake-up to be detected, there must only be a rising edge and a long enough logic 1 level.

0 件の賞賛
返信