On the bottom side of the MC33772B, there is a 5.4 mm × 5.4 mm exposed metal area.
However, the PCB design guide recommends a solder mask opening of only 3.7–3.8 mm, which suggests an EPAD size of about 3.7 mm.
In actual inspection, the exposed metal area on the IC bottom is 5.4 mm, which is larger than the recommended PCB opening.
According to the datasheet, the region from 3.7 mm (min) to 5.4 mm (max) is specified as a PCB routing keep-out area.
If 3.7 mm is the recommended EPAD size and the 3.7–5.4 mm region is defined as a PCB routing keep-out area, what is the reason that this whole region is designed as exposed metal on the bottom side of the package?