MC33730 linear regulators

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33730 linear regulators

2,290 Views
Gelby
Contributor III

Hello all,

I'm going to use the MC3370 chip in an environment where I need only the 5V and the 3.3V voltages.

I don't need to use any stand by supplies, I know the VKAM is always active (also with the chip in sleep mode) and this is ok for me, I want to use VDDL as 3.3V source and I don't need more.

To save power in stand by, I want to program the VDD3 regulator as 3.3V, not stand by regulator, but I don't need it because I use the VDDL regulator as 3.3V source, here my question, have I to add the external pass NPN transistor and bypass capacitors to the VDD3 circuitry (VDD3_B and VDD3), or can I simply left open these two pins (VDD3_B and VDD3)?

Thanks a lot,

Regards.

Alessandro

0 Kudos
Reply
2 Replies

2,228 Views
Gelby
Contributor III

Thank you G.w. Sun,

so there isn't at all the risk to damage the linear regulator or may be the entire chip?, I mean, the stage that should drive the external pass transistor (may be an op amp?) works always in saturation because of the absence of the feedback voltage, I think..

Regards,

Alessandro

0 Kudos
Reply

2,228 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI Alessandro

After discussed ,to be on safe consider please add the external pass NPN transistor and bypass capacitors to the VDD3 circuitry (VDD3_B and VDD3) if unused this LDO

0 Kudos
Reply