MC33664 TPL data bits 0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33664 TPL data bits 0

Jump to solution
1,790 Views
divyam
Contributor II

Hi,

I'm trying to communicate to MC33771 AFE and while debugging i noticed that whatever I send on MOSI_TX, the TPL waveform bits are logic 0 only (attached waveform)


tpl_0_data.png

image.png

Also: -

1. Wakeup function is working properly. When TPL wakeup command is sent, VCOM changes from 0V to 5V 
2. Waiting for 5msec after sending the wakeup command, before sending any command on SPI_TX 
3. Trying to debug BCC_AssignCid(), whatever data is being sent on SPI_MOSI_TX, TPL shows 0 logic pulses only (corresponding to SPI RX waveform)

Right now i want to focus on the MC33664 transceiver only.
The transceiver should transmit the corresponding data on the bus, in both the cases (AFE present, AFE absent) ?

MC33664

0 Kudos
Reply
1 Solution
1,736 Views
divyam
Contributor II

Hi Jozef,

We tested the same on another hardware.
(Vio = 3.29V, VCC5 = 5.01V)

The data bit stream is OK in that.

This thread can be closed.


View solution in original post

0 Kudos
Reply
3 Replies
1,776 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Divyam,

please share your schematic with voltage levels and part values.

With Best Regards,

Jozef

0 Kudos
Reply
1,737 Views
divyam
Contributor II

Hi Jozef,

We tested the same on another hardware.
(Vio = 3.29V, VCC5 = 5.01V)

The data bit stream is OK in that.

This thread can be closed.


0 Kudos
Reply
1,770 Views
divyam
Contributor II

Hi Jozef,

Please find the info below:

tpl_sch.png

VCC5     = 4.88V
VIO        = 3.25V
RDTX+  = 2.51V (idle)
RDTX-   = 2.49V (idle)

The waveform shown previously is b/w (RDTX+ and RDTX- after the signal transformer, on the AFE side)

MPN = MC33664ATL1EG

Tags (1)
0 Kudos
Reply