Linux driver for PF1550 and iMX6ULZ

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Linux driver for PF1550 and iMX6ULZ

4,457 次查看
ian3
Contributor II

Hi

Could somebody clarify which linux driver to use for the the PF1550 with the iMX6ULZ and where I can find an example device tree binding.

Thanks

Ian

标签 (2)
4 回复数

4,351 次查看
norman_stetter
Contributor I

I too would like to know what the status of the PF1550 driver is.

0 项奖励
回复

4,413 次查看
Yuri
NXP Employee
NXP Employee

[email protected] 

Hello,

  PMIC PF1550 is supported by NXP Linux BSP.  Use section 2.5.2 (PMIC PF Regulator)

of i.MX Linux Reference Manual (Rev. L5.4.24_2.1.0) for more details.

Embedded Linux for i.MX Applications Processors | NXP 

Regards,

Yuri.

0 项奖励
回复

4,413 次查看
ian3
Contributor II

Hi

In L5.4.24_2.1.0 I see the pf1550-regulator-rpmsg driver but not the pf1550 client driver. I just checked and the client driver was available in the 4.19.35_1.1.0 release (pf1550.c) but has been removed in latest BSP. I also noticed the pf1550 charger driver was removed in the latest release, pf1550-charger.c in /drivers/power/supply. 

Do I have to use the rpmsg drive now, even in a iMX6ULZ application? What about the battery charger driver as that has now been removed?

Thanks

Ian

0 项奖励
回复

4,317 次查看
Yuri
NXP Employee
NXP Employee

@ian3 
Hello,

  Yes, It has been removed from  L5.4.24_2.1.0 release. However, if customers are using pf1550 with i.MX6ULZ then they can still port/integrate those drivers in their BSP. The BSP team has been requested about  reasons behind the removal of the driver; I will inform You  in case of an update.

Regards,
Yuri.