LLC+PPC Converter design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LLC+PPC Converter design

2,945 Views
Sakthi_Ed
Contributor I

Hello there,

We are designing a new PSU unit with TEA2016 controller to convert 230C AC to 12V (18A) & 5V (2.5A) DC with an overall power rating of 230W. 

Based on the reference designs and design calculator tools available from NXP, we are facing a few difficulties in the selection of the below-mentioned components. Could you please help us find the suitable devices asap? 

1. Boost inductor,

2. Resonant inductor ( in LLC topology )

3. Primary inductor integrated with transformer (dual secondary transformer + auxillary 18V winding).

Could you please share with us the exact part number or custom-made part drawings that we can get from the manufacturers and kickstart our project asap?

Thanks,
Sakthivel

0 Kudos
Reply
1 Reply

2,920 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Sakthivel,

The PFC coil(s) and LLC transformer on the TEA2016DB1519 240W demo board are from supplier Würth Elektronik. Samples for development purposes can be requested via the website.

For India and South East Asia area you can contact Kiran Irugu ([email protected])

The TEA2016DB1519 board uses the same components as the TEA1916DB1262 board. I attached the specifications.

NXP TEA19161T | Demoboard TEA1916DB1262 | Würth Elektronik Reference Design Search

image004.pngimage004.png

NXP TEA19162T | Demoboard TEA1916DB1262 | Würth Elektronik Reference Design Search

image001.pngimage001.png

BRs, Tomas

0 Kudos
Reply