Inquiry regarding RDBESS774A3EVB - Board Damage due to Swapped Connectors (J1_1 and J1_3)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inquiry regarding RDBESS774A3EVB - Board Damage due to Swapped Connectors (J1_1 and J1_3)

324 Views
WcrTh
Contributor II

Hi,

I am currently evaluating the RDBESS774A3EVB Cell Monitoring Unit (CMU) board (which features the MC33774A Battery Cell Controllers) connected to a 50-cell battery pack setup.

Recently, an accidental misconnection occurred during our testing. We mistakenly swapped the cell connector sets between J1_1 (upper set) and J1_3 (lower set).

The following behaviors were observed during the incident:

  1. Initial Event: Immediately upon swapping the connectors, a heavy short circuit occurred at Cell 36, causing an external wire/trace to burn out and break.

  2. Subsequent Action: After discovering the mistake, we reconnected the battery packs to the same board using the correct connector positions.

  3. Secondary Behavior: As soon as the correct connection was established, multiple balancing resistors (R_balance) on the board began to overheat and burn out.

Based on this scenario, we would highly appreciate your engineering insights regarding the following questions:

  • Q1: Did the initial connector swap between J1_1 and J1_3 cause catastrophic internal damage to the MC33774A ICs or related circuitry during the first event?

  • Q2: Is it correct to assume that the multiple balancing resistors burning out during the second (correct) connection was a direct consequence of internal damage inside the MC33774A ICs (e.g., internal FET breakdown or gate drivers stuck in an ON-state) caused by the first incident?

  • Q3: If we replace the damaged MC33774A ICs and all the burned balancing resistors, can the RDBESS774A3EVB board be restored to a fully functional and safe working condition? Are there any other critical companion components (such as ESD/Zener protection diodes or isolation circuit elements) that we should inspect or replace alongside the main ICs?

Tags (2)
0 Kudos
Reply
3 Replies

315 Views
guoweisun
NXP TechSupport
NXP TechSupport

guoweisun_0-1782106495796.png

Do you mean you mistake to add the 50*3.6V voltage between C17 to ground in the MC33774 first part?

0 Kudos
Reply

155 Views
WcrTh
Contributor II

Hi  @guoweisun,

To ensure complete hardware safety and prevent any potential wiring issues, we have designed a intermediate "CSU BRIDGE BOARD" to route our 50S battery pack to the RDBESS774A3EVB (featuring three MC33774A AFEs in a daisy chain).

Could you please review our attached schematics (CSUBridge_Connector.png and CSUBridge_Block Diagram.png) and verify if our pin mapping and connection strategy are correct?

 

CSUBridge_Block Diagram.png

CSUBridge_Connector.png

0 Kudos
Reply

284 Views
WcrTh
Contributor II

Hi @guoweisun,

We did not connect the entire 50-cell pack into a single connector. Instead, our 50-cell system is divided into three separate segments with three distinct cell connectors.

1 Initial Event ERROR: CONNECTOR SWAP1 Initial Event ERROR: CONNECTOR SWAP2 Subsequent Action: NORMAL CONNECTION2 Subsequent Action: NORMAL CONNECTION

Tags (2)
0 Kudos
Reply