The 24 V is the stable output from the SMPS power supply for the first step test. However, the real system will be replaced with a battery one. I would like to confirm which supply voltage range is most suitable for the GD3160.
Since the device includes an internal regulator from VSUP to 5 V, operating at 24 V will result in higher power dissipation compared to 12 V due to the larger voltage drop across the internal regulator.
Could you please confirm whether using 24 V as VSUP is acceptable from a thermal and reliability standpoint, or if 12 V would be a better operating condition for this device?