FS85: About MCU fault recovery strategy

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS85: About MCU fault recovery strategy

726件の閲覧回数
Kojimaa
Contributor III

Hi NXP,

  What I want to know about this strategy is whether FS0B automatically becomes high after meeting the recovery conditions, or does it need to be released again via software ?

Thank you  in advance

タグ(1)
0 件の賞賛
返信
3 返答(返信)

720件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

When the fail-safe outputs FS0B is asserted low by the device due to a fault, the exit

conditions must be validated before allowing these pins to be released.

These conditions are:

  • Fault is removed
  • LBIST_OK = ABIST1_OK = ABIST2_OK = 1
  • Fault Error Counter = 0
  • RELEASE_FS0B register filled with ongoing WD_SEED reversed and complemented
0 件の賞賛
返信

708件の閲覧回数
Kojimaa
Contributor III

Hello,

    Do I also need to release FS0B again via software after FCCU recovered during the recovery window?

 

0 件の賞賛
返信

692件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

For the SBC side to release FS0B:

  • Fault is removed
  • LBIST_OK = ABIST1_OK = ABIST2_OK = 1
  • Fault Error Counter = 0
  • RELEASE_FS0B register filled with ongoing WD_SEED reversed and complemented

 

Firstly fault should be removed, then read the related registers to make sure LBIST_OK = ABIST1_OK = ABIST2_OK = 1 and Fault error counter=0 then fill the RELEASE_FS0B registers to release FS0B.

0 件の賞賛
返信