FS4500 wake up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS4500 wake up

3,134件の閲覧回数
ydygcvjhbjkjnkn
Contributor I

Asking for help

Now I am using FS4500, I want to go to sleep and use 1145CAN transceiver to wake up. The INH of the transceiver is connected to IO_0 of the SBC board. Using the host computer to send the wake-up frame packet, the INH pin of the 1145CAN transceiver changes from low output to high output, and the IO_0 pin of the SBC board will also change accordingly. The question is whether I need to use the ICU driver to capture the interrupt and exit sleep or another way, or if the IO_0 pin changes accordingly, the register value will be updated automatically. Quit sleep? Asking for help

0 件の賞賛
返信
4 返答(返信)

3,127件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

I think that you do not need the ICU driver. Once configured properly (IO_0 connected to INH, WU_IO0_1:0 = 0b01 ), the FS4500 will autonomously wake up from sleep when IO_0 transitions (e.g. when INH goes high in response to a specific CAN frame).

BRs, Tomas

0 件の賞賛
返信

3,118件の閲覧回数
ydygcvjhbjkjnkn
Contributor I
Thank you for your answer,
However, after I set the 1145 transceiver to sleep mode and FS4500 also enters LPOFF mode, I use the host computer to send CAN packets. The register CW of the 1145 transceiver is read and set to 1, indicating that the 1145 transceiver has detected the wake-up event. At this time, the INH pin of the 1145 transceiver should have a high or low change (because the device pin is not well tested, not tested), but the FS4500 can not execute the subsequent code after sleeping through the SPI command, I understand that it is not awake, want to ask the big brother, what should I do
0 件の賞賛
返信

3,085件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

If CW bit is set, wake-up was successful on TJA1145 side. Try probing the INH pin with an oscilloscope or logic analyzer to confirm if it goes from low to high (~VBAT) after the wake-up event. If INH does not toggle high, FS4500 will not detect a wake source on IO_0 and will remain in LPOFF.

If INH pin behavior is ok, double check your IO_0 pin configuration as a wake-up capable input before entering LPOFF. Otherwise, FS4500 will not detect the INH signal change and will not leave LPOFF.

BRs, Tomas

0 件の賞賛
返信

3,122件の閲覧回数
ydygcvjhbjkjnkn
Contributor I
谢谢你的解答,
不过我现在在将1145收发器设置为睡眠模式后,FS4500也进入LPOFF模式后,使用上位机发送CAN报文,读取到1145收发器的寄存器CW置为1,表示1145收发器检测到唤醒事件,此时1145收发器的INH引脚应该会有高低变化(因器件引脚不好测试,未测试),不过FS4500在通过SPI指令睡眠之后,仍然不能执行后续代码,我理解的也就是还未唤醒,想要请教大佬,我应该怎么做
0 件の賞賛
返信