FS26 PMIC VPRE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS26 PMIC VPRE

3,023 Views
GNANAPANDI
Contributor I

Hai NXP Team,

we design Motor Controller using S32K311 Microcontroller With FS26 PMIC,

We config FS 26 PMIC as Direct Voltage from Battery voltage to VSUP pin. we don't used VBST connection so VBST_FB, VBST_ISL, VBST_ISH connected to GND as per datasheets.

Now only we get voltage VDIG =1.5V, VBOS =5.0V, VPRE =0V

what we do to get VPRE voltage ???

 

0 Kudos
Reply
5 Replies

2,998 Views
GNANAPANDI
Contributor I

MFS2613AMD3D and MFS2613AMD6D

0 Kudos
Reply

2,995 Views
guoweisun
NXP TechSupport
NXP TechSupport

MFS2613AMDA3AD and MFS2613AMDA6AD,right? If yes they are frond-end configuration you need refer to below circuit:

guoweisun_0-1722412061297.pngguoweisun_0-1722412061297.png

 

0 Kudos
Reply

2,974 Views
GNANAPANDI
Contributor I

if this PMIC , will it support direct power supply to VSUP without Front end mode (without VBST) configuration 

 

0 Kudos
Reply

2,955 Views
guoweisun
NXP TechSupport
NXP TechSupport

No,for these two parts had done OTP with the frond-end model which doesn't support this.

0 Kudos
Reply

3,000 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

What's your detail FS26 part number?

0 Kudos
Reply