FS26:Is the MCU fault recovery strategy only effective for S32K3xx?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS26:Is the MCU fault recovery strategy only effective for S32K3xx?

723件の閲覧回数
Kojimaa
Contributor III

Hi,

  Im using FS26xyD with TC3xx and was enabled by OTP, but this mechanism seems to be ineffective. When FCCU input is activated, RSTB asserted immediately .

Kojimaa_0-1700706395979.png

 

Thank you in advance

0 件の賞賛
返信
3 返答(返信)

709件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

In your MCU side there is no FCCU pins,right? if no FCCU,you need disable FCCU function in SBC side.

guoweisun_0-1700717827126.png

 

0 件の賞賛
返信

695件の閲覧回数
Kojimaa
Contributor III

Hi,

   TC3XX has an FSP similar to FCCU that can be monitored, but this MCU recovery strategy seems do not work.

 

0 件の賞賛
返信

688件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

For the SBC side if you want to use the FCCU function, you need do below two points:

1: hardware connection: according the FCCU_CFG bit setting to design this connection

guoweisun_0-1700791931750.png

 

2: registers setting:

FS_I_SAFE_INPUTS register and FS_I_NOT_SAFE_INPUTS (0x48)

0 件の賞賛
返信