FS26:Is the MCU fault recovery strategy only effective for S32K3xx?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS26:Is the MCU fault recovery strategy only effective for S32K3xx?

668 Views
Kojimaa
Contributor III

Hi,

  Im using FS26xyD with TC3xx and was enabled by OTP, but this mechanism seems to be ineffective. When FCCU input is activated, RSTB asserted immediately .

Kojimaa_0-1700706395979.png

 

Thank you in advance

0 Kudos
Reply
3 Replies

654 Views
guoweisun
NXP TechSupport
NXP TechSupport

In your MCU side there is no FCCU pins,right? if no FCCU,you need disable FCCU function in SBC side.

guoweisun_0-1700717827126.png

 

0 Kudos
Reply

640 Views
Kojimaa
Contributor III

Hi,

   TC3XX has an FSP similar to FCCU that can be monitored, but this MCU recovery strategy seems do not work.

 

0 Kudos
Reply

633 Views
guoweisun
NXP TechSupport
NXP TechSupport

For the SBC side if you want to use the FCCU function, you need do below two points:

1: hardware connection: according the FCCU_CFG bit setting to design this connection

guoweisun_0-1700791931750.png

 

2: registers setting:

FS_I_SAFE_INPUTS register and FS_I_NOT_SAFE_INPUTS (0x48)

0 Kudos
Reply