Establishing SPI communication between Two MC33771 and Master Controller Unit.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Establishing SPI communication between Two MC33771 and Master Controller Unit.

2,910件の閲覧回数
Autoven
Contributor I

Hello all,

I am using MC33771 for BMS development, for 16 cell battery.
MC33771 is 14 channel cell controller. Thus using two of them, eight channel from each MC33771 cell controller. 

These two MC33771 cell controller will be communicating through SPI with the Master Controller.
Master Controller has two SPI Modules say, SPI A and SPI B,

The question is, is it OK to connect the SPI A of MCU with MC33771 Cell Controller and SPI B of MCU with other MC33771 cell controller.
If it is connected will the battery get shorted in the MCU, because it will be having a common ground for both SPI lines.

0 件の賞賛
返信
1 返信

2,881件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Autoven,

Have you considered using two parallel MC33771 devices with the same SPI bus but with different chip selects?

 

Regards,

David

0 件の賞賛
返信