Hi
I have a "imk93 11x11 EVK" card
on Yocto , i have done the following commands
# echo 1 > /sys/devices/platform/imx93-lpm/mode
# cat /sys/devices/platform/imx93-lpm/mode
System is in ND mode with DDR 1866 MTS!
# mhz
1398 MHz, 0.7153 nanosec clock
# echo 0 > /sys/devices/platform/imx93-lpm/mode
# mhz
1690 MHz, 0.5917 nanosec clock
Unfortunatelly echo 2 and echo 3 dosn't work
i have to change nodes in the dts tree to add these 2 modes
Where ares the dst files i have to change ?
Where ares the nodes i have to change in the dst files ?
greetings