Current measurement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Current measurement

Jump to solution
3,231 Views
Gad_usr1
Contributor II

Hi, how can we measure current of battery pack using RD33771CDSTEVB and BATT14C emulator.  Where should we connect the shunt resistor and in which channel in BATT 14c emulator is the current measurement done. Kindly clarify.

Tags (1)
0 Kudos
Reply
1 Solution
3,162 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello

So for your desired two function I think you can refer to EVB -RD33771-48VEVM.

RD33771-48VEVM Reference Design | NXP Semiconductors 

View solution in original post

0 Kudos
Reply
4 Replies
3,143 Views
Gad_usr1
Contributor II

Thank you. Is there any limit on the current sense for this board? For example can it support a battery pack of 48V, 200Ah

0 Kudos
Reply
3,215 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

For this RD33771CDSTEVB,the shunt current detection pins are connected with ground.

 

ErikaC_1-1719506951047.png

So, I think you can refer to FRDM33771CSPEVB 

Regards.

0 Kudos
Reply
3,198 Views
Gad_usr1
Contributor II

We are using this along with MPC5775B-EVB as part of the MPC5775B and MC33771 high-voltage BMS Evaluation System. MPC57775B-EVB supports only TPL.  Is there any other board of MC33771C which has TPL and current sensing both enabled. I believe  FRDM33771CSPEVB supports only SPI.

Tags (1)
0 Kudos
Reply
3,163 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello

So for your desired two function I think you can refer to EVB -RD33771-48VEVM.

RD33771-48VEVM Reference Design | NXP Semiconductors 

0 Kudos
Reply