Configuration issues with FS26, and reasons for initialization failures

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuration issues with FS26, and reasons for initialization failures

7,226件の閲覧回数
MNN
Contributor II

Hello:
I am using fs26 for the first time, and encountered some problems when using FS26_B0_4.4_1.0.0_CD01. My Sbc_fs26_InitDevice() returns NOT_OK. I have not made any changes to the Sbc_fs26 module, I would like to ask what does the instance in the figure below represent? I also want to ask, is there a possible reason why Sbc_fs26_InitDevice() returns NOT_OK?

hfma_0-1686101291141.pnghfma_1-1686101324333.png

 

ラベル(2)
0 件の賞賛
返信
7 返答(返信)

7,205件の閲覧回数
MNN
Contributor II

是驱动软件,从官网下载的RTD。运行在自己的板子上,运行的是驱动是Sbc_fs26_TS_T40D34M10I0R0。自己板子和FS26连接的SPI脚和提供的案例中的SPI脚也是一样的。

0 件の賞賛
返信

7,196件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

你能判断SBC现在在什么状态吗?还是在INIT的状态吗?出错是哪里出错?

0 件の賞賛
返信

7,186件の閲覧回数
MNN
Contributor II

刚才使用了EVB板子,还是初始化错误。错误的函数是Sbc_fs26_InitDevice。SBC应该是在

INIT状态

0 件の賞賛
返信

7,162件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

是喂狗错误吗?能查到counter error是多少吗?

确定FS26是simple 还是challenge的喂狗方式?再看看喂狗的程序给的值是不是对的,这是两种不同的喂狗方式

0 件の賞賛
返信

7,142件の閲覧回数
MNN
Contributor II
使用自己项目板子时,无法用Sbc_fs26_ReadRegister读取寄存器的值。使用的spi设置是正确的,sbc_fs26模块没有做任何修改。不明白什么原因。
0 件の賞賛
返信

7,181件の閲覧回数
MNN
Contributor II
使用的是s32k344
0 件の賞賛
返信

7,215件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

FS26_B0_4.4_1.0.0_CD01这个是驱动软件吗?您是再什么板子上跑的这个驱动?是EVB还是自己做的板子?

 

0 件の賞賛
返信