5600 development board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

5600 development board

3,288 Views
quanwang
Contributor I

The 5600 development board purchased on the official website is supplied with 12V power supply. After burning the 5600 chip through the normal operation process, when using user_mode to verify the chip output voltage, the current of the development board is more than 2A abnormal, and the normal value should be 12mA. May I ask if there is any problem with the burning board that needs to be repaired, or is there any other verification scheme

Tags (1)
0 Kudos
Reply
7 Replies

3,271 Views
guoweisun
NXP TechSupport
NXP TechSupport

5600是你自己做的OTP吗?做过OTP以后上电就有2A的静态电流这么大?

 

 

0 Kudos
Reply

3,269 Views
quanwang
Contributor I
通过GUI软件自己配置的OTP,只有烧录OTP后 进入user mode 或检测输出电压 电源显示2.5A电流 我们之前的烧录板就只有12mA 用新买的就是2.5A 操作流程和配置的OTP是一致的 可能是哪里的问题??
0 Kudos
Reply

3,265 Views
guoweisun
NXP TechSupport
NXP TechSupport

在没有负载的情况下12V的电源电流到了2.5A?

你看看后面接负载了吗?

0 Kudos
Reply

3,262 Views
quanwang
Contributor I
没负载,烧录板外部没任何负载 和之前前的烧录板一样 烧录成功后 只测输出 电压 检测芯片烧录成功是否 外部无任何负载 只是测一下电压正常就可以 但现在新买的烧录板 烧录完后的软件 电流过高 烧录板型号和之前12mA的烧录板一样
0 Kudos
Reply

3,254 Views
guoweisun
NXP TechSupport
NXP TechSupport

2.5A的静态电流不正常可能要把芯片烧坏或者已经坏掉了。

烧录板是我们官方的socket板子吗?

0 Kudos
Reply

3,251 Views
quanwang
Contributor I
是的 SKTEVM板子
0 Kudos
Reply

3,248 Views
guoweisun
NXP TechSupport
NXP TechSupport

那你还是换回来以前的板子烧录吧,我估计是板子除了问题。

0 Kudos
Reply