tdm bus speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tdm bus speed

1,372 Views
Pamid
Contributor II

What is the maximum speed that TDM bus can support with p1021

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,286 Views
alexander_yakov
NXP Employee
NXP Employee

The following is said in QE reference Manual, Section 22.2:

The P1021/P1012/ P1025/P1016 supports TDM in a high-speed mode. To run in this mode, the QUICC
Engine platform to TDM interface frequency ratio should be 8:1, where a ratio of 400 MHz:50 MHz is
recommended. The TDM maximum frequency is 50 MHz.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply