question about P2020 U-boot TLB setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

question about P2020 U-boot TLB setting

2,028 Views
hyoungkikim
Contributor IV

i have a difficult time to configure u-boot  to a new board

( i am not  good at english ^^)

i am porting u-boot to a new board which is based on P2020RDB-PC

the board has MRAM device and external uart chips which was connected to eLBC

i configured LAWS and related registers

but i have no clue about TLB

in u-boot   there is a tlb.c in  P2020RDB board related files

and in that file   tbl_table is defined

is this necessary to include new device into that table ?

if so, how ?

just  copy one entry to new one and  modify just address ?

and what about kernel  ?  where do i configure TLB ?

thanks in advnace

Labels (1)
2 Replies

1,680 Views
bpe
NXP Employee
NXP Employee

>is this necessary to include new device into that table ?

>if so, how ?

[Platon] If you need to do anything with your peripherals in u-Boot

environment, then yes, you have to set a TLB for them. Some of our

development systems have board-level control registers connected to

the local bus, see how TLBs are defined for them, do the same. You take a

look how macros PIXIS_BASE, PIXIS_BASE_PHYS are used in in

/board/freescale/p1022ds/tlb.c for instance.

If your peripherals are to be used in Linux only, then it is OK not

to setup a TLB for them (LAW is still necessary).

>and what about kernel  ?  where do i configure TLB ?

[Platon] Linux kernel creates a mapping for a peripheral when it's

driver calls ioremap().


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,680 Views
hyoungkikim
Contributor IV

thank you   it is really of great help

0 Kudos
Reply