p2041 srio type11 send issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

p2041 srio type11 send issue

2,304 次查看
yinux
Contributor III

I send a packet(8 bytes) of type11  to the target, the target received 2 packets(16bytes), then the sender Outbound Message Hardware Errors shows "Segment Response Time-Out Errors".

Follow the p2041RM document.

111.png

there are some questions.

  1. how to send the “RESPONSE without data” msg?  what is meaning of the ttpye?  I cannot find any introduce from the p2041 document and DPAARM document.
  2. Follow the DPAARM document
    1. a) I send a packet of type10, then the target received 2 packets.
    2. b) I send a packet of type9, then the target received 1 packets.

What is differences?

  1. I want to use the type6 ,outbound and inbound mode, the p2041 cannot support the

inbound mode, which cpu can support it?

标记 (1)
0 项奖励
回复
1 回复

1,964 次查看
yang_lei
Contributor II

How did you send the msg/doorbell ? Using RMU ?

0 项奖励
回复