eTSEC1 reset configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eTSEC1 reset configuration

2,258件の閲覧回数
dank4
Contributor II

i want to set the eTSEC1 at POR to act at MII mode , 

according to Table 3-2 at the P2020RM the cfg_tsec1_prtcl[0,1] are TSEC1_TXD[0,7] signals respectively.

according to Table 4-19 in order to work as MII the POR values should be :

cfg_tsec_reduce = 1 , and cfg_tsec1_prtcl = 01.

it is not clear to me

does that mean cfg_tsec1_prtcl = TSEC1_TXD[0,7] = 01 ?

i would expect the notion to be cfg_tsec1_prtcl[0:1] = 01 

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,210件の閲覧回数
ufedor
NXP Employee
NXP Employee

prtcl.jpg

2,211件の閲覧回数
dank4
Contributor II

thank you

0 件の賞賛
返信