boot p1013 from spi flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

boot p1013 from spi flash

1,103件の閲覧回数
somyaaggarwal08
Contributor II

Hi,

I want to boot p1013 based card from spi flash . Can we program spi flash using jtag interface? Could you provide some jtag script file to do so?

ラベル(1)
0 件の賞賛
返信
1 返信

1,022件の閲覧回数
ufedor
NXP Employee
NXP Employee

To program SPI Flash It is possible to use CodeWarrior Flash Programmer.

0 件の賞賛
返信