With SETA=1 is the external LGTA exempt from the bus monitor?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

With SETA=1 is the external LGTA exempt from the bus monitor?

跳至解决方案
709 次查看
sapril
Contributor I

Hi -

I am using a P1020 with the local bus configured with SETA = 1 for CS4. 

The manual says for sure that if SETA = 1, ONLY LGTA can terminate a transaction; internal TA is completely ignored.

So, does that mean that External TA is exempt from bus monitor? 

标签 (1)
标记 (6)
0 项奖励
回复
1 解答
621 次查看
LPP
NXP Employee
NXP Employee

When SETA =1 then an access is terminated either by LGTA assertion or by

the bus monitor whatever happens earlier.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
622 次查看
LPP
NXP Employee
NXP Employee

When SETA =1 then an access is terminated either by LGTA assertion or by

the bus monitor whatever happens earlier.

0 项奖励
回复
621 次查看
alexander_yakov
NXP Employee
NXP Employee

In case if internal TA generation is disabled by SETA, local bus GPCM controller will wait for external TA (LGTA) assertion.

If there is no external TA assertion within reasonable time, bus monitor will terminate this transaction and generate TEA ("transfer error acknowledge").