Using SEC 4.4 on P1010 from bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using SEC 4.4 on P1010 from bootloader

1,683件の閲覧回数
alexandernovik2
Contributor II

Hello!

I'am trying to understand SEC 4.4 and how to use it from bootloader (simple custom bootloader, written with assembly). I just need to compute CRC of boot image but I can't find some code examples to figure out how to start. Is there any examples how to use it?

ラベル(1)
タグ(3)
1 返信

1,540件の閲覧回数
bpe
NXP Employee
NXP Employee

The recommended way to perform a CRC or hash operation over memory is
by constructing and submitting a Job Descriptor via the Job Ring
interface. Below is a  simple descriptor to calculate a CRC over a
contiguous block of memory:

 [00] B0800009       jobhdr: stidx->[00] len=9
 [01] 8490002C    operation: cls2-op crc ietf3385 init-final dec
 [02] 24540000       fifold: class2 msg-last2 ext
 [03] 00000000               ptr->@0x0fdec4080
 [04] FDEC4080
 [05] 00449D00               extlen=4496640
 [06] 54200004          str: ccb2-ctx len=4 offs=0
 [07] 00000000               ptr->@0x0feb95140
 [08] FEB95140

Simple routines for creating and managing SEC jobs can be found in
u-Boot SEC driver:

http://git.freescale.com/git/cgit.cgi/ppc/sdk/u-boot.git/tree/drivers/crypto/fsl?id=fsl-sdk-v2.0-170...