Unable to verify CAN functionality on P1010RDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to verify CAN functionality on P1010RDB

2,587 Views
fahadarslan
Contributor II

Hi,

While trying to verify CAN functionality using two P1010RDB targets following error is encountered.

irq 16: nobody cared (try booting with the "irqpoll" option)

Updated hwconfig in uboot is

=> print hwconfig

hwconfig=fsl_p1010mux:tdm_can=can;usb1:dr_mode=host,phy_type=utmi

And to configure dtb and kernel to support CAN, following FSL link has been followed:

Freescale Technical Information Center

From output of /proc/interrupts before and after sending CAN frames, there is no increment in irq count registered for can0 (irq number 48) instead irq count for irq number 16 increases to 100000 and irq 16: nobody cared (try booting with the "irqpoll" option) error message is observed.

Observed same behavior on both P1010RDB and P1010RDB-PB

Kindly see the log below:

.

.

.

Poky (Yocto Project Reference Distro) 1.6 p1010rdb-pb /dev/ttyS0

p1010rdb-pb login: root

root@p1010rdb-pb:~#

root@p1010rdb-pb:~# ifconfig -a

can0      Link encap:UNSPEC  HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00 

          NOARP  MTU:16  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:10

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

          Interrupt:48

can1      Link encap:UNSPEC  HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00 

          NOARP  MTU:16  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:10

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

          Interrupt:61

dummy0    Link encap:Ethernet  HWaddr 7e:56:88:93:14:37 

          BROADCAST NOARP  MTU:1500  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

eth0      Link encap:Ethernet  HWaddr 00:04:9f:03:44:6e 

          inet addr:137.202.157.11  Bcast:137.202.157.255  Mask:255.255.254.0

          inet6 addr: fe80::204:9fff:fe03:446e/64 Scope:Link

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:14698 errors:0 dropped:0 overruns:0 frame:0

          TX packets:9602 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:11133237 (10.6 MiB)  TX bytes:2196416 (2.0 MiB)

          Base address:0x2000

eth1      Link encap:Ethernet  HWaddr 00:04:9f:03:44:6f 

          BROADCAST MULTICAST  MTU:1500  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

          Base address:0x4000

eth2      Link encap:Ethernet  HWaddr 00:04:9f:03:44:70 

          BROADCAST MULTICAST  MTU:1500  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

          Base address:0x6000

lo        Link encap:Local Loopback 

          inet addr:127.0.0.1  Mask:255.0.0.0

          inet6 addr: ::1/128 Scope:Host

          UP LOOPBACK RUNNING  MTU:65536  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

sit0      Link encap:UNSPEC  HWaddr 00-00-00-00-00-01-00-00-00-00-00-00-00-00-00-00 

          NOARP  MTU:1480  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

tunl0     Link encap:IPIP Tunnel  HWaddr  

          NOARP  MTU:0  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

root@p1010rdb-pb:~#

root@p1010rdb-pb:~#

root@p1010rdb-pb:~# cat /proc/interrupts

           CPU0      

16:          0   OpenPIC    16 Level     [PCI] PME, [PCI] PME, fsl-ifc

17:          2   OpenPIC     0 Level     phy_interrupt

19:         19   OpenPIC    19 Level     fsl-ifc-nand

20:          0   OpenPIC    20 Level     fsldma-chan

21:          0   OpenPIC    21 Level     fsldma-chan

22:          0   OpenPIC    22 Level     fsldma-chan

23:          0   OpenPIC    23 Level     fsldma-chan

28:        383   OpenPIC    28 Level     ehci_hcd:usb1

29:       9418   OpenPIC    29 Level     eth0_g0_tx

30:       9804   OpenPIC    30 Level     eth0_g0_rx

34:          0   OpenPIC    34 Level     eth0_g0_er

41:          0   OpenPIC    41 Level     fsl-sata

42:        443   OpenPIC    42 Level     serial

43:          0   OpenPIC    43 Level     i2c-mpc, i2c-mpc

45:          2   OpenPIC    45 Level     ffe31000.jr, ffe32000.jr, ffe33000.jr, ffe34000.jr

59:       1442   OpenPIC    59 Level     fsl_espi

68:          0   OpenPIC    68 Level     gianfar_ptp

74:          0   OpenPIC    74 Level     fsl-sata

LOC:       4472   Local timer interrupts

SPU:          0   Spurious interrupts

PMI:          0   Performance monitoring interrupts

MCE:          0   Machine check exceptions

root@p1010rdb-pb:~# ip link set can0 up type can bitrate 125000 ;

flexcan ffe1c000.can can0: bitrate error 0.0%

flexcan ffe1c000.can can0: writing ctrl=0xc7112001

root@p1010rdb-pb:~#

root@p1010rdb-pb:~#

root@p1010rdb-pb:~#

root@p1010rdb-pb:~# cat /proc/interrupts

           CPU0      

16:          0   OpenPIC    16 Level     [PCI] PME, [PCI] PME, fsl-ifc

17:          2   OpenPIC     0 Level     phy_interrupt

19:         19   OpenPIC    19 Level     fsl-ifc-nand

20:          0   OpenPIC    20 Level     fsldma-chan

21:          0   OpenPIC    21 Level     fsldma-chan

22:          0   OpenPIC    22 Level     fsldma-chan

23:          0   OpenPIC    23 Level     fsldma-chan

28:        460   OpenPIC    28 Level     ehci_hcd:usb1

29:       9510   OpenPIC    29 Level     eth0_g0_tx

30:      10077   OpenPIC    30 Level     eth0_g0_rx

34:          0   OpenPIC    34 Level     eth0_g0_er

41:          0   OpenPIC    41 Level     fsl-sata

42:        574   OpenPIC    42 Level     serial

43:          0   OpenPIC    43 Level     i2c-mpc, i2c-mpc

45:          2   OpenPIC    45 Level     ffe31000.jr, ffe32000.jr, ffe33000.jr, ffe34000.jr

48:          0   OpenPIC    48 Level     can0

59:       1442   OpenPIC    59 Level     fsl_espi

68:          0   OpenPIC    68 Level     gianfar_ptp

74:          0   OpenPIC    74 Level     fsl-sata

LOC:       4685   Local timer interrupts

SPU:          0   Spurious interrupts

PMI:          0   Performance monitoring interrupts

MCE:          0   Machine check exceptions

root@p1010rdb-pb:~#

root@p1010rdb-pb:~# ip link set can1 up type can bitrate 125000 ;                                                                                                                

flexcan ffe1d000.can can1: bitrate error 0.0%

flexcan ffe1d000.can can1: writing ctrl=0xc7112001

root@p1010rdb-pb:~#

root@p1010rdb-pb:~#

root@p1010rdb-pb:~# cat /proc/interrupts

           CPU0      

16:          0   OpenPIC    16 Level     [PCI] PME, [PCI] PME, fsl-ifc

17:          2   OpenPIC     0 Level     phy_interrupt

19:         19   OpenPIC    19 Level     fsl-ifc-nand

20:          0   OpenPIC    20 Level     fsldma-chan

21:          0   OpenPIC    21 Level     fsldma-chan

22:          0   OpenPIC    22 Level     fsldma-chan

23:          0   OpenPIC    23 Level     fsldma-chan

28:        503   OpenPIC    28 Level     ehci_hcd:usb1

29:       9531   OpenPIC    29 Level     eth0_g0_tx

30:      10180   OpenPIC    30 Level     eth0_g0_rx

34:          0   OpenPIC    34 Level     eth0_g0_er

41:          0   OpenPIC    41 Level     fsl-sata

42:        758   OpenPIC    42 Level     serial

43:          0   OpenPIC    43 Level     i2c-mpc, i2c-mpc

45:          2   OpenPIC    45 Level     ffe31000.jr, ffe32000.jr, ffe33000.jr, ffe34000.jr

48:          0   OpenPIC    48 Level     can0

59:       1442   OpenPIC    59 Level     fsl_espi

61:          0   OpenPIC    61 Level     can1

68:          0   OpenPIC    68 Level     gianfar_ptp

74:          0   OpenPIC    74 Level     fsl-sata

LOC:       4806   Local timer interrupts

SPU:          0   Spurious interrupts

PMI:          0   Performance monitoring interrupts

MCE:          0   Machine check exceptions

root@p1010rdb-pb:~# cansend can0 123#1122334455667788

-sh: cansend: command not found

root@p1010rdb-pb:~# ca

cal            caller         cantest        case           cat            cat.coreutils  catv          

root@p1010rdb-pb:~# cantest  can0 123#1122334455667788

irq 16: nobody cared (try booting with the "irqpoll" option)

CPU: 0 PID: 2470 Comm: cantest Not tainted 3.12.19-rt30-QorIQ-SDK-V1.6+gc29fe1a #1

Call Trace:

[effefef0] [c0006bd4] show_stack+0x44/0x15c (unreliable)

[effeff30] [c0073b9c] __report_bad_irq.isra.6+0x38/0xf4

[effeff50] [c0073e78] note_interrupt+0x1a8/0x268

[effeff80] [c0071e94] handle_irq_event_percpu+0x138/0x1c4

[effeffc0] [c0071f54] handle_irq_event+0x34/0x54

[effeffd0] [c0074cb0] handle_fasteoi_irq+0xa0/0x154

[effeffe0] [c000436c] __do_irq+0x48/0x74

[effefff0] [c000ca88] call_do_irq+0x24/0x3c

[ef693e20] [c00043fc] do_IRQ+0x64/0xb4

[ef693e40] [c000e3fc] ret_from_except+0x0/0x18

--- Exception: 501 at put_pid+0x0/0x48

    LR = __fput+0xc8/0x214

[ef693f00] [c00d43d8] __fput+0x9c/0x214 (unreliable)

[ef693f20] [c0058af8] task_work_run+0xac/0xf0

[ef693f40] [c000e9b8] do_user_signal+0x74/0xc4

--- Exception: c00 at 0xff0b9cc

    LR = 0x10000644

handlers:

[<c001ac64>] fsl_pci_pme_handle

[<c001ac64>] fsl_pci_pme_handle

[<c001da74>] fsl_ifc_ctrl_irq

Disabling IRQ #16

root@p1010rdb-pb:~# lsmod

Module                  Size  Used by

root@p1010rdb-pb:~# cat /proc/interrupts

           CPU0      

16:     100000   OpenPIC    16 Level     [PCI] PME, [PCI] PME, fsl-ifc

17:          2   OpenPIC     0 Level     phy_interrupt

19:         19   OpenPIC    19 Level     fsl-ifc-nand

20:          0   OpenPIC    20 Level     fsldma-chan

21:          0   OpenPIC    21 Level     fsldma-chan

22:          0   OpenPIC    22 Level     fsldma-chan

23:          0   OpenPIC    23 Level     fsldma-chan

28:        761   OpenPIC    28 Level     ehci_hcd:usb1

29:       9612   OpenPIC    29 Level     eth0_g0_tx

30:      10960   OpenPIC    30 Level     eth0_g0_rx

34:          0   OpenPIC    34 Level     eth0_g0_er

41:          0   OpenPIC    41 Level     fsl-sata

42:        986   OpenPIC    42 Level     serial

43:          0   OpenPIC    43 Level     i2c-mpc, i2c-mpc

45:          2   OpenPIC    45 Level     ffe31000.jr, ffe32000.jr, ffe33000.jr, ffe34000.jr

48:          1   OpenPIC    48 Level     can0

59:       1442   OpenPIC    59 Level     fsl_espi

61:          0   OpenPIC    61 Level     can1

68:          0   OpenPIC    68 Level     gianfar_ptp

74:          0   OpenPIC    74 Level     fsl-sata

LOC:       5685   Local timer interrupts

SPU:          0   Spurious interrupts

PMI:          0   Performance monitoring interrupts

MCE:          0   Machine check exceptions

root@p1010rdb-pb:~# uname -a

Linux p1010rdb-pb 3.12.19-rt30-QorIQ-SDK-V1.6+gc29fe1a #1 Thu Dec 18 14:58:52 PKT 2014 ppc GNU/Linux

root@p1010rdb-pb:~#

root@p1010rdb-pb:~#

root@p1010rdb-pb:~# dmesg | grep -i can

[    0.944863] CAN device driver interface

[    0.948157] flexcan ffe1c000.can: device registered (reg_base=f10b6000, irq=48)

[    0.954864] flexcan ffe1d000.can: device registered (reg_base=f10b8000, irq=61)

[    0.967612] mdio_bus mdio@ffe24000: cannot get PHY at address 3

[    1.317013] can: controller area network core (rev 20120528 abi 9)

[    1.325106] can: raw protocol (rev 20120528)

[    1.328087] can: broadcast manager protocol (rev 20120528 t)

[    1.332453] can: netlink gateway (rev 20130117) max_hops=1

[   94.002516] flexcan ffe1c000.can can0: bitrate error 0.0%

[   94.007087] flexcan ffe1c000.can can0: writing ctrl=0xc7112001

[   94.011646] flexcan ffe1c000.can can0: flexcan_set_bittiming: mcr=0x5980000f ctrl=0xc7112001

[   94.011652] flexcan ffe1c000.can can0: flexcan_chip_start: writing mcr=0x79a20208

[   94.011657] flexcan ffe1c000.can can0: flexcan_chip_start: writing ctrl=0xc711ec51

[   94.011663] flexcan ffe1c000.can can0: flexcan_chip_start: reading mcr=0x60a20208 ctrl=0xc711ec51

[  103.766575] flexcan ffe1d000.can can1: bitrate error 0.0%

[  103.771094] flexcan ffe1d000.can can1: writing ctrl=0xc7112001

[  103.775650] flexcan ffe1d000.can can1: flexcan_set_bittiming: mcr=0x5980000f ctrl=0xc7112001

[  103.775656] flexcan ffe1d000.can can1: flexcan_chip_start: writing mcr=0x79a20208

[  103.775661] flexcan ffe1d000.can can1: flexcan_chip_start: writing ctrl=0xc711ec51

[  103.775667] flexcan ffe1d000.can can1: flexcan_chip_start: reading mcr=0x60a20208 ctrl=0xc711ec51

[  138.012392] CPU: 0 PID: 2470 Comm: cantest Not tainted 3.12.19-rt30-QorIQ-SDK-V1.6+gc29fe1a #1

[  138.099233] flexcan ffe1c000.can can0: Error Warning IRQ

[  138.099240] flexcan ffe1c000.can can0: Error Passive IRQ

[  138.099244] flexcan ffe1c000.can can0: bus-off

root@p1010rdb-pb:~#

Thanks,

Fahad

Labels (1)
0 Kudos
Reply
4 Replies

2,250 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Fahad Arslan,

Please make sure that two CAN controllers have been connected with straight serial cable correctly, otherwise you will encounter the above error. (On p1010RDB CAN_L and CAN_H signals connect to the correspondent signals for the other CAN controller, please refer to the hardware user guide).

For example, on P1010RDB-PA, if the user want to attach CAN1 and CAN0 on the same board, the connection should be like the following.

J17-2 to J15-2

J17-7 to J15-7

In addition, before send the CAN frames with cantest  can0 123#1122334455667788, please set up the listen process on the other board( or CAN controller) with “cantest can*”.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,250 Views
fahadarslan
Contributor II

Hi Yiping,

Yes, I'm using straight serial cable and I've confirmed the connections using multimeter but still facing the same issue.

Thanks,

Fahad

0 Kudos
Reply

2,250 Views
fahadarslan
Contributor II

Hi Pavel,

Thanks for looking into this.

As I mentioned above, I've already tried updating hwconfig in uboot :

=> print hwconfig

hwconfig=fsl_p1010mux:tdm_can=can;usb1:dr_mode=host,phy_type=utmi

If you meant to drop specifying usb in hwconfig , I've just tried following but it didn't work either:

=> print hwconfig                                                                                                                                        

hwconfig=fsl_p1010mux:tdm_can=can

Regards,

Fahad

0 Kudos
Reply