UBOOT for P1020

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UBOOT for P1020

2,363 Views
belenieamoranto
Contributor I

Hello,

Where do I find the UBOOT for the P1020?

Thanks,

Belenie

Labels (1)
0 Kudos
Reply
3 Replies

1,849 Views
addiyi
NXP Employee
NXP Employee

Depend on whitch version of P1020 board you are using. For P1020rdb you can findfsl02bba9uild uboot image at this link. You have to download QorIQ-SDK-V1.5-PPCE500V2-IMAGE , then follow the steps from infocenter.

Adrian

0 Kudos
Reply

1,849 Views
scottwood
NXP Employee
NXP Employee

Note that p1020rdb is supported upstream, so another option is to get the latest upstream release from Denx.  Regardless of where you get the source code, make sure you choose the right U-Boot target for the board revision (P1020RDB-PC, P1020RDB-PD, or the non-suffixed target for PB).

0 Kudos
Reply

1,849 Views
belenieamoranto
Contributor I

Thanks for the information :smileyhappy:

0 Kudos
Reply