Hi all,
I am working on a P1023 integrated board. Where DTSEC2 connected to a Ethernet PHY (that goes via Serdes-lane 03.... / lanes numbers from 0 to 3) is working fine.
But DTSEC1(that goes via SerDes lane 02) to ARM based marvel switch, without any PHY connection between them.
I checked switch is working fine. SerDes-lane 02 connection is good.
I removed the "auto negotiation enable" inorder to support phyless connection at uboot and still we have problem.
-------------------------------------------------
drivers/net/tsec.c
I removed TBICR_ANEG_ENABLE option from TBICR_ANEG_ENABLE macro
The edited one looks like this.
#ifndef CONFIG_TSEC_TBICR_SETTINGS
#define CONFIG_TSEC_TBICR_SETTINGS ( \
TBICR_PHY_RESET \
/* TBICR_ANEG_ENABLE */
| TBICR_FULL_DUPLEX \
| TBICR_SPEED1_SET \
)
#endif /* CONFIG_TSEC_TBICR_SETTINGS */
----------------------------------------------------
Is there is any better ways to resolve the issue.
Regards,
Sarath
已解决! 转到解答。
Welcome. And more comment from application:
there should be some setting in the switch side, to have the switch port to work at phy-less mode. In other words, make both the DTSEC and switch port to work at MAC-to-MAC mode.
You could check the link status on both the TBI MDIO register at DTSEC side, and switch port side, to make sure both side has the link-up status.
Then set the switch port to work at echo mode/loopback mode to narrow down the problem.
Thank you lunminliang. Now i am able to connect switch in U-Boot and soon kernel bring up I lost connection.
Any how I am making changes in DTS according to your referred link. Update you soon I got connectivity.
Welcome. And more comment from application:
there should be some setting in the switch side, to have the switch port to work at phy-less mode. In other words, make both the DTSEC and switch port to work at MAC-to-MAC mode.
You could check the link status on both the TBI MDIO register at DTSEC side, and switch port side, to make sure both side has the link-up status.
Then set the switch port to work at echo mode/loopback mode to narrow down the problem.
Hi Albert,
Make sure the settings
Step 1:
drivers/net/tsec.c
I removed TBICR_ANEG_ENABLE option from TBICR_ANEG_ENABLE macro
The edited one looks like this.
#ifndef CONFIG_TSEC_TBICR_SETTINGS
#define CONFIG_TSEC_TBICR_SETTINGS ( \
TBICR_PHY_RESET \
/* TBICR_ANEG_ENABLE */
| TBICR_FULL_DUPLEX \
| TBICR_SPEED1_SET \
)
#endif /* CONFIG_TSEC_TBICR_SETTINGS */
Step 2:
In your dts change the tsec of your mdio to tbi PHY.
mdio0: mdio@e1120 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,fman-mdio";
reg = <0xe1120 0xee0>;
interrupts = <26 1 0 0>;
tbi0: tbi-phy@8 {
reg = <0x8>;
device_type = "tbi-phy";
};
};
Check you PHY address in the following:
=> mii info
PHY 0x04: OUI = 0x5043, Model = 0x1C, Rev = 0x00, 10baseT, HDX
PHY 0x05: OUI = 0x5043, Model = 0x1C, Rev = 0x00, 10baseT, HDX
PHY 0x06: OUI = 0x5043, Model = 0x1C, Rev = 0x00, 10baseT, HDX
PHY 0x07: OUI = 0x5043, Model = 0x1C, Rev = 0x00, 10baseT, HDX
PHY 0x08: OUI = 0x0000, Model = 0x00, Rev = 0x00, 1000baseX, FDX
PHY 0x09: OUI = 0x5043, Model = 0x1C, Rev = 0x00, 10baseT, HDX
PHY 0x0A: OUI = 0x5043, Model = 0x1C, Rev = 0x00, 10baseT, HDX
PHY 0x0B: OUI = 0x5043, Model = 0x1C, Rev = 0x00, 10baseT, HDX
In this ours is PHY 0x08.
You may take a look at thisDevice Tree (.dts) configuration for eTSEC2 in SGMII/Serdes mode