Running Linux on 8GB P5020

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Running Linux on 8GB P5020

1,697 Views
adriancox
Contributor III

I'm running our P5020 board with 8GB of memory, and having a number of problems with Linux. Our kernel is based off the sdk-v1.5 tag in the Freescale GIT tree. With 4GB of memory every driver worked, but with 8GB the following drivers have failed: MMC, USB, and SATA. In each case the on-chip device only supports 32-bit addressing.

I've fixed MMC by disabling DMA when the board has more than 4GB. Has anybody got USB and SATA working in large memory scenarios?

usb 1-1: device descriptor read/64, error -32

usb 1-1: device descriptor read/64, error -32

usb 1-1: new high-speed USB device number 3 using fsl-ehci

usb 1-1: device descriptor read/64, error -32

usb 1-1: device descriptor read/64, error -32

usb 1-1: new high-speed USB device number 4 using fsl-ehci

usb 1-1: device not accepting address 4, error -32

usb 1-1: new high-speed USB device number 5 using fsl-ehci

usb 1-1: device not accepting address 5, error -32

hub 1-0:1.0: unable to enumerate USB device on port 1

ata2: Signature Update detected @ 504 msecs

ata2: SATA link up 3.0 Gbps (SStatus 123 SControl 300)

ata2.00: failed to IDENTIFY (INIT_DEV_PARAMS failed, err_mask=0x80)

ata2: limiting SATA link speed to 1.5 Gbps

ata2: Signature Update detected @ 504 msecs

ata2: SATA link up 3.0 Gbps (SStatus 123 SControl 300)

ata2.00: failed to IDENTIFY (INIT_DEV_PARAMS failed, err_mask=0x80)

ata2: Signature Update detected @ 504 msecs

ata2: SATA link up 3.0 Gbps (SStatus 123 SControl 300)

Labels (1)
Tags (4)
0 Kudos
Reply
1 Reply

1,363 Views
adriancox
Contributor III

Fixed it - in moving to our own board file a typo had disabled SWIOTLB initialisation for platform devices.

0 Kudos
Reply