Re-Imaging P1020WLAN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Re-Imaging P1020WLAN

2,590 次查看
erwinw
Contributor III

Are there detailed instructions on how to re-image the flash of the P1020 WLAN rev D? Are the files available in the P1020WLAN Software bundle with the factory image?

标签 (1)
2 回复数

2,354 次查看
arashaz_
Contributor II

Hi again,

There is a VB script called tftpdown-p1020wlan-nor.vbs in the USB disk provided by Freescale. You can have a look.

Arash

2,354 次查看
arashaz_
Contributor II

Hello,

If you like to put a new U-boot, I am not sure . But, if you like only to change the Linux image:

Build your Linux image using LTIB or SDK. It provides you a uImage file, a Ramdisk file and a .dtb file. Note that all these files for the default Linux installed are available in the USB provided by the device.

Then, using hyperterminal (windows) or minicom (linux), go to U-boot command line (stop normal booting). By TFTP, put those three files in the RAM and boot from RAM. If the image worked well, You can reboot and put the files in the NOR Flash in default addresses. If you use “printenv” in U-boot, you can see the default addresses (you should make the protect off). I recommend you to make a copy of your NOR Flash before trying to write in the flash. For the RAM boot, you can write the following commands in U-boot CLI, one by one:

setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate ramdisk_size=200000

tftp $ramdiskaddr $ramdiskfile

tftp $loadaddr $bootfile

tftp $fdtaddr p1020wlan_rev_d.dtb

bootm $loadaddr $ramdiskaddr 0xc00000


The files in your TFTP folder should be called: uImage , p1020wlan_rev_d.dtb and rootfs.ext2.gz.uboot


I hope it helps.

Arash