QorIQ processor in new project.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QorIQ processor in new project.

3,271件の閲覧回数
eugene_volkov
Contributor I

Hello.

In my plane, use QorIQ  processor in new project.

I'm interested, the QorIQ processor line will be updated by the NXP company in the coming years?

0 件の賞賛
返信
4 返答(返信)

2,709件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Please look our recent presentation from FTF forum for the information about further processors in Networking Product segment.

https://community.nxp.com/servlet/JiveServlet/downloadBody/334911-102-1-276069/AMF-NET-T2732.pdf 


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,709件の閲覧回数
eugene_volkov
Contributor I

Hello, Alexander.

QorIQ Power architectures will develop in further? 

0 件の賞賛
返信

2,709件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

If you mean QorIQ processors based on Power Architecture, than - according to our recent product roadmap presentation, we dont have plans to announce new processors based on Power Architecture for this moment, but factory team is working on increasing speeds and decreasing power consumption by 10-20% for existing Power Architecture T4xxx devices. New devices will have "1" at the end of partnumber and collectively mentioned as "T4xx1". For more information please search our public web site by "introducing T4xx1" keyword.

0 件の賞賛
返信

2,709件の閲覧回数
robertoinnocent
Contributor III

In fact there are already (from some months) these chip T4xx1 upgraded and even the T208x chips that have the same reduced power consumption,

T2 Family Low Power Options|NXP 

so I hope the factory team is working on the T chips with 14nm fabrication dimension like the Layerscape ARM new processors, and possibly with Sata3 and Usb3 and DDR4 support.

0 件の賞賛
返信