Power Down Cycle

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power Down Cycle

1,526件の閲覧回数
danielminors
Contributor I

In the datasheet  P1011EC, P1011 QorIQ Integrated Processor Hardware Specification section 2.3 Power Down Requirements it states;

"The power-down cycle must complete such that power supply values are below 0.4 V before a new power-up cycle can be started."

Is this true for all the power rails or just the Core and platform supply voltage and PLL supply?

ラベル(1)
0 件の賞賛
返信
1 返信

1,327件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Yes, this requirement is for all power supplies.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信