PCIe current requirements

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCIe current requirements

1,122件の閲覧回数
toddreed
Contributor I

How can I find/determine the current requirements for:

SVDD_1.05V SerDes Core Supply

XVDD_1.05V SerDes Pad Supply

for a P2020 using all 4 lanes of PCIe (x1, x1, x2)?

Thanks,

Todd

ラベル(1)
0 件の賞賛
返信
1 返信

1,038件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

For your configuration PCIe (x1, x1, x2) estimated power numbers are 0.38W (SVDD) + 0.13W (XVDD) = 0.51W


Have a great day,
Andrei

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信