P4080 UL94 Certification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P4080 UL94 Certification

1,593 Views
Sebster
Contributor II

Hi NXP support,

I'm after the P4080 UL94 flammability report. Could you provide that to me please?

Thanks
SPA

Labels (1)
0 Kudos
Reply
1 Reply

1,403 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

I know that there are P4080 based boards wich meet UL 94 V-0 flammability rating, but I did not see P4080 UL94 flammability report on the NXP intranet and website. There is UL Online Certifications Directory.

http://www.ul.com/database 

You may use the UL Online Certifications Directory to:

⦁    Verify a UL Certification, Classification, or Recognition

⦁    Verify a UL Listed product use

⦁    Verify a UL Recognized component use

⦁    Verify a product safety standard

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply