P4080 PCie Keyboard input error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P4080 PCie Keyboard input error

1,320 Views
gopikrishnan
Contributor III

Recently we procured an P4080 PCie. After set-up we could see uboob console and linux boot-up. But we could not able to issue commands through the keyboard. We used minicom on /dev/ttyS0 to view the console. attached the log file for your reference:

Original Attachment has been moved to: u-boot.console.txt.zip

Labels (1)
0 Kudos
Reply
1 Reply

1,164 Views
Pavel
NXP Employee
NXP Employee

Do you use the minicom as console?

The P4080 u-boot uses console for output and input.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply