P4080 PCie Keyboard input error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P4080 PCie Keyboard input error

1,319件の閲覧回数
gopikrishnan
Contributor III

Recently we procured an P4080 PCie. After set-up we could see uboob console and linux boot-up. But we could not able to issue commands through the keyboard. We used minicom on /dev/ttyS0 to view the console. attached the log file for your reference:

Original Attachment has been moved to: u-boot.console.txt.zip

ラベル(1)
0 件の賞賛
返信
1 返信

1,163件の閲覧回数
Pavel
NXP Employee
NXP Employee

Do you use the minicom as console?

The P4080 u-boot uses console for output and input.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信