P4080 DTSEC FIFO Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P4080 DTSEC FIFO Issue

2,766件の閲覧回数
sharper
Contributor III

After a couple of hours running SNMP traffic, the DTSEC only reports DROPPED packets.

Could this be the result of a FIFO overflow/buffer management issue?

What steps should be taken to help diagnose the cause and/or prevent it from occurring?

Thanks!

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,464件の閲覧回数
sharper
Contributor III

Is there a control/status register somewhere that might help pin down the problem?

0 件の賞賛
返信

2,464件の閲覧回数
bpe
NXP Employee
NXP Employee

RDRP os a low-level conter, it increments for any dropped frame.

There is another counter, RODC, which counts frames dropped due to

no buffer condition. See DPAARM, Section 8.4.4.3.33. Note that Fman

can be configured to send pause frames when it detects a buffer pool

depletion, see Section 8.4.6.18.3. For other error types that may

cause frames to be dropped see Sections 8.3.7 and 8.4.6.18.

Registers that can help in finding the root cause of the problem

are FM_EPI and     various BMI statistic counters, see Table 8-42, offsets

from 0x200 and the corresponding register description.

Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信