P4080 DTSEC FIFO Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P4080 DTSEC FIFO Issue

2,706 Views
sharper
Contributor III

After a couple of hours running SNMP traffic, the DTSEC only reports DROPPED packets.

Could this be the result of a FIFO overflow/buffer management issue?

What steps should be taken to help diagnose the cause and/or prevent it from occurring?

Thanks!

Labels (1)
0 Kudos
Reply
2 Replies

2,404 Views
sharper
Contributor III

Is there a control/status register somewhere that might help pin down the problem?

0 Kudos
Reply

2,404 Views
bpe
NXP Employee
NXP Employee

RDRP os a low-level conter, it increments for any dropped frame.

There is another counter, RODC, which counts frames dropped due to

no buffer condition. See DPAARM, Section 8.4.4.3.33. Note that Fman

can be configured to send pause frames when it detects a buffer pool

depletion, see Section 8.4.6.18.3. For other error types that may

cause frames to be dropped see Sections 8.3.7 and 8.4.6.18.

Registers that can help in finding the root cause of the problem

are FM_EPI and     various BMI statistic counters, see Table 8-42, offsets

from 0x200 and the corresponding register description.

Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply