P2041 Local bus timing question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2041 Local bus timing question

1,095件の閲覧回数
gradymuldrow
Contributor I

I'm designing local bus interface from P2041 processor to some Flash and nVSRAM parts.  In the QorIQ P2040 Reference Manual, Rev 4 section 13.4.2.3.4, it states that the LOE_B asserts and negates on the rising edge of the bus clock, but this conflicts with the waveforms in Figures 13-14, 13-15 where it is shown changing on falling edge of clock.  Which is correct?  Thanks, Grady

ラベル(1)
0 件の賞賛
返信
1 返信

973件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Reference Manual figures are for illustration purposes only. Please look P2041 Hardware Specifications, Figure 22 for exact reference point from which LOE assertion/negation is measured, and Table 51 for delay values.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信