P2020 and 88E6046 communication with RGMII interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2020 and 88E6046 communication with RGMII interface

1,237件の閲覧回数
wyt_uestc
Contributor I

Hi Dear:

    I use P2020 tsec1 RGMII port  to connect Marvell's 88E6046 switch .The 88E6046's PHY port connect to PC.The P2020 can receive data from PC,but the PC can not receive data when P2020 send data.I have tested the RGMII signal ,and not find abnormal.

ラベル(1)
0 件の賞賛
返信
1 返信

1,096件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please check:

1) quality of the EC _GTX_CLK125 referring the P2020 QorIQ Integrated Processor Hardware Specifications, 2.4.4 eTSEC Gigabit Reference Clock Timing.

2) the PHY documentation and its registers to ensure that internal delay for the RXC is enabled.

0 件の賞賛
返信