P1020 Not Booting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P1020 Not Booting

2,810 次查看
akashjain
Contributor I
Hello
We are trying to P1020 using SD card and follow error is soming
SD boot...
Dram: initialising..., spd disabled in config
SPD error on controller 0! Trying fallback to raw timing calculation
DDR: using modified new Timings...1024tbd_HCH9-FULL01
Second program loader running in sram...
Kindly help us debug this issue.

标记 (1)
0 项奖励
回复
4 回复数

2,648 次查看
akashjain
Contributor I

Hi

Also in come boards i am getting the following while booting

Kindly Look into this

## Resetting to default environment
Saving Environment to MMC...
Writing to MMC(0)... done
2925 bytes read in 66 ms (43 KiB/s)
 
## Checking Image at 01000000 ...
   Legacy image found
   Image Name:   Demo Script File
   Created:      2018-04-25   9:20:32 UTC
   Image Type:   PowerPC Linux Script (uncompressed)
   Data Size:    2861 Bytes = 2.8 KiB
   Load Address: 00000000
   Entry Point:  00000000
   Contents:
      Image 0: 2853 Bytes = 2.8 KiB
   Verifying Checksum ... OK
## Executing script at 01000000
-x-x-x-x-x RM U-Boot-PROD.SCR_2017 TYPE-B SWITCH v2.1ef x-x-x-x-x-
-x-x-x-x-x Updating U-Boot environments x-x-x-x-x-
xxx Environment variable norbootaddr = ec000000 xxxx norfdtaddr = eff00000
-x-x-x-x-x Updating System images x-x-x-x-x-
adding new environments
Erasing uboot environments
Error: end address (0xeff3ffff) not in flash!
Bad address format
Error: end address (0xeff3ffff) not in flash!
Bad address format
131072 bytes read in 79 ms (1.6 MiB/s)
Error: end address (0xeff3ffff) not in flash!
Bad address format
failed to erase env
Updating Uboot@ eff40000 xxx
786432 bytes read in 134 ms (5.6 MiB/s)
Error: end address (0xefffffff) not in flash!
Bad address format
Error: end address (0xefffffff) not in flash!
Bad address format
Error: end address (0xefffffff) not in flash!
Bad address format
byte at 0x01000000 (0x27) != byte at 0xeff40000 (0xe7)
Total of 0 byte(s) were the same
failed to update u-boot
Updating uImage@ ec000000 xxx
2523161 bytes read in 214 ms (11.2 MiB/s)
Error: end address (0xec268018) not in flash!
Bad address format
Error: end address (0xec268018) not in flash!
Bad address format
Error: end address (0xec268018) not in flash!
Bad address format
byte at 0x01000000 (0x27) != byte at 0xec000000 (0xe4)
Total of 0 byte(s) were the same
failed to update u-boot
xxx Updating setenv_img@ 0xefee0000 xxx
1234 bytes read in 62 ms (18.6 KiB/s)
Error: end address (0xefee04d1) not in flash!
Bad address format
Error: end address (0xefee04d1) not in flash!
Bad address format
Error: end address (0xefee04d1) not in flash!
Bad address format

0 项奖励
回复

2,648 次查看
Pavel
NXP Employee
NXP Employee

Look at attached u-boot configuration file from SDK 1.9 for the P1020. Enable SPD for DDR initialization. See attachment.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,648 次查看
akashjain
Contributor I

yes found the attachment, so Pavel what we are facing is that we have almost 15-20 boards assembled so we are facing the issue in 2-3 boards.

We are using all same files for all the boards.

Can you guide us in this. 

0 项奖励
回复

2,648 次查看
akashjain
Contributor I

Hello 

I can not find any attachment .

0 项奖励
回复