P1011: Generating PCIe TLP Packet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1011: Generating PCIe TLP Packet

1,224 Views
anthonyellis
Contributor I

Hi,

If I wished to use memory write operations to fill a FIFO rather than use DMA will the PCIe controller in the P1011 generate a single TLP transaction with a sixteen byte data field if the write transaction was  targeted to a data type defined to be of type 4 x 32 bit.

Thanks Anthony

Labels (1)
0 Kudos
Reply
1 Reply

1,041 Views
ufedor
NXP Employee
NXP Employee

The request is not clear.

1) You wrote:

> memory write operations to fill a FIFO

Which exactly operation is in question?

2) You wrote:

> data type defined to be of type 4 x 32 bit

What exactly do you mean?

0 Kudos
Reply