P1011: Generating PCIe TLP Packet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1011: Generating PCIe TLP Packet

1,242件の閲覧回数
anthonyellis
Contributor I

Hi,

If I wished to use memory write operations to fill a FIFO rather than use DMA will the PCIe controller in the P1011 generate a single TLP transaction with a sixteen byte data field if the write transaction was  targeted to a data type defined to be of type 4 x 32 bit.

Thanks Anthony

ラベル(1)
0 件の賞賛
返信
1 返信

1,059件の閲覧回数
ufedor
NXP Employee
NXP Employee

The request is not clear.

1) You wrote:

> memory write operations to fill a FIFO

Which exactly operation is in question?

2) You wrote:

> data type defined to be of type 4 x 32 bit

What exactly do you mean?

0 件の賞賛
返信