Monitoring the L3 cache on P4080

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Monitoring the L3 cache on P4080

1,529 Views
clemensreibetan
Contributor I

Hi,

is there any way to monitor the L3 cache on the P4080?

Some Performance Monitor Counters that count cache misses or something like this?

Thanks in advance.

Regards

Clemens

Labels (1)
0 Kudos
Reply
1 Reply

1,146 Views
LPP
NXP Employee
NXP Employee

P4080 Event Processing Unit (EPU) supports monitoring of CoreNet L3 Cache CPC Events and of DDR transactions Received from CoreNet and CPC.

The fuctionality is described in separate documents for advanced QorIQ Debug and Performance Monitoring. Support is limited to 3rd Party Tool vendors and you need to contact a Freescale representative (or create a Service Request) to get access to this documents.

Customers (not tool developers) wishing to use this debug feature set are enabled via CodeWarrior and 3rd party tools. CodeWarrior provides Performance analysis tool. It allows user to select events and counters for analysis. Please refer to CW documentation : "Tracing and Analysis Tools User Guide".

A customer can use QorIQ Debug feature set without CW or third party tools by using SPID Library API. Customer should contact FSL to engage in a service contract to be enabled with SPID Library.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply