“Is it necessary that the nodes shown in "lspci" output, have to be defined in device tree ?
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hi,
“Is it necessary that the nodes shown in "lspci" output, have to be defined in device tree ? I have device tree file for P2041RDB. In that only one node is created for pci i.e. bus 0. Now I have customized the reference board and connected one pcie-pci bridge to bus 0 and four pci devices are connected to that bridge. So in my lspci output, six node is showing. So is it necessary that I have to declare it all in device tree.”
regards,
Avinash

- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hello Avinash,
No need to define PCIe devices in the device tree. In fact, only PCIe controllers are defined in the dts file.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Thanks for your response Yiping.
One thing I also want to clear is that if it is necessary to declare the pcie/pci devices, if so, how is the interrupt number assigned to them. I have a dts for pci controllrer bellow,
pci1: pcie@ffe201000 {
reg = <0xf 0xfe201000 0 0x1000>;
ranges = <0x2000000 0x0 0xe0000000 0xc 0x20000000 0x0 0x20000000
0x1000000 0x0 0x0 0xf 0xf8010000 0x0 0x10000>;
compatible = "fsl,p2041-pcie", "fsl,qoriq-pcie-v2.2", "fsl,qoriq-pcie";
device_type = "pci";
#size-cells = <2>;
#address-cells = <3>;
bus-range = <0 0xff>;
clock-frequency = <33333333>;
interrupts = <16 2 1 14>;
fsl,iommu-parent = <&pamu0>;
fsl,liodn-reg = <&guts 0x504>;
pcie@0{
ranges = <0x2000000 0 0xe0000000 0x2000000
0 0xe0000000 0 0x20000000
0x1000000 0 0x0 0x1000000
0 0x0 0 0x10000>;
reg = <0 0 0 0 0>;
#interrupt-cells = <1>;
#size-cells = <2>;
#address-cells = <3>;
device_type = "pci";
interrupts = <16 2 1 14>;
interrupt-map-mask = <0xf800 0 0 7>;
interrupt-map = <
0 0 0 1 &mpic 41 1 0 0
0 0 0 2 &mpic 5 1 0 0
0 0 0 3 &mpic 6 1 0 0
0 0 0 4 &mpic 7 1 0 0 >;
};
};
The output of lspci -t is
-[0000:00]---00.0-[01-07]----00.0-[02-07]--+-01.0-[03]----00.0
+-02.0-[04-05]----00.0-[05]--+-00.0
| +-01.0
| +-02.0
| \-03.0
+-03.0-[06]----00.0
\-04.0-[07]----00.0
When I execute the "lspci -vvv" command all my device are assigned with an interrupt number, how is this interrupt number assigned, how should I modify the interrupt number, cause i'm experiencing an interrupt failure when I run the device tester program. How should I do the interrupt mapping for this assembly?

- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Interrupt specifiers consists of 4 cells encoded as follows:
<1st-cell> interrupt-number
Identifies the interrupt source. The meaning
depends on the type of interrupt.
Note: If the interrupt-type cell is undefined
(i.e. #interrupt-cells = 2), this cell
should be interpreted the same as for
interrupt-type 0-- i.e. an external or
normal SoC device interrupt.
<2nd-cell> level-sense information, encoded as follows:
0 = low-to-high edge triggered
1 = active low level-sensitive
2 = active high level-sensitive
3 = high-to-low edge triggered
<3rd-cell> interrupt-type
The following types are supported:
0 = external or normal SoC device interrupt
The interrupt-number cell contains
the SoC device interrupt number. The
type-specific cell is undefined. The
interrupt-number is derived from the
MPIC a block of registers referred to as
the "Interrupt Source Configuration Registers".
Each source has 32-bytes of registers
(vector/priority and destination) in this
region. So interrupt 0 is at offset 0x0,
interrupt 1 is at offset 0x20, and so on.
1 = error interrupt
The interrupt-number cell contains
the SoC device interrupt number for
the error interrupt. The type-specific
cell identifies the specific error
interrupt number.
2 = MPIC inter-processor interrupt (IPI)
The interrupt-number cell identifies
the MPIC IPI number. The type-specific
cell is undefined.
3 = MPIC timer interrupt
The interrupt-number cell identifies
the MPIC timer number. The type-specific
cell is undefined.
<4th-cell> type-specific information
The type-specific cell is encoded as follows:
- For interrupt-type 1 (error interrupt),
the type-specific cell contains the
bit number of the error interrupt in the
Error Interrupt Summary Register.
Please also refer to "Advanced Interrupt Mapping" in Device Tree Usage - eLinux.org .
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------