How to run a simple program on P4080DS Hypervisor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to run a simple program on P4080DS Hypervisor

1,154件の閲覧回数
peterzheng
Contributor II

Hi,

I have successfully deployed Hypervisor in SDK 1.6 onto the P4080DS Board. When I boot up, it will show the terminal of Hypervisor like

"HV>".

The project I am doing now requires me to run some simple program, for example, "hello world", on P4080DS hypervisor to study the functions of hypervisor and feature of P4080DS, including

  1. Cache locking & Partitioning
  2. System partitioning
  3. Corenet Fabric partitioning (BUS)
  4. Core to DDR mapping (static).

In this case, I could not find documentation on how to compile and run such simple program on p4080DS hypervisor. Do I need to use Codewarrior for this purpose?

Thanks & Regards,

Peter Zheng

ラベル(1)
タグ(2)
0 件の賞賛
返信
0 返答(返信)